Pollution category

The POL category aims to prevent and control pollution and surface water run-off in association with a building’s location and use. By following the parameters in this category, you reduce your building’s impact on surrounding communities and the environment. Possible pollution includes light-pollution as well as noise, flooding and emissions to air, land and water

Are you keen to discuss your upcoming project?

Get a consultancy from ABB Experts

POL1 – Impact of refrigerants– max 4 credits AIM - To reduce the level of greenhouse gas emissions arising from the leakage of refrigerants used to heat or cool the building.

Assessment criteria:

  • Leak detection: Where systems using refrigerants have a permanent automated refrigerant leak detection system installed

ABB Smart Buildings Solutions

(*) Part of leak detection system.​

Refrigerant metering could be an input into a controller but this is not normally a category considered as part of a BEMS control system.​

POL4 – Nighttime light pollution – max 1 credit  AIM - To ensure that external lighting is concentrated in the appropriate areas and that upward lighting is minimized, reducing unnecessary obtrusive light pollution, energy consumption and nuisance to neighboring properties

Assessment criteria:

  • All external lighting (except for safety and security lighting) can be automatically switched off between 23:00 and 07:00

ABB Smart Buildings Solutions

(*) Applicable for the devices that can switch external lighting​

(**) All Metering products (except CMS and EV meters) have digital outputs that can act for controlling an on/off switch, Control can be carried out by timers (AG timers, DBT timers) and by twilight switches (TL line). Dimming is not possible

Energy metering

Find out more

Door entry system​

Find out more

HVAC

Find out more

Connectivity to BMS​

Find out more

Conventional wiring accessories and installation materials

Find out more

Building Automation KNX ​

Find out more