— The Solution

Together, Hamburger Hochbahn AG and ABB installed a turnkey solution that included the installation of a transformer, switchgear and 44 heavy vehicle charging stations with 150 kW power each.

To maintain the existing footprint, much of the electrification equipment was located on the terminal roof, delivering a space saving of around 30%.

To complete the transition to electric, ABB delivered the planning and implementation of the electric infrastructure and the connection of the bus depot to the grid.