—

The Challenge

With the 45,000 m2 Dalmine manufacturing site already being supplied with 100% green energy from renewable sources, it was necessary to identify other areas where efficiencies could be made to reduce carbon emissions and achieve ABB’s Mission to Zero status.

The Objectives

The core objective for the Dalmine circuit breaker and switchgear facility were:

  • Reduce CO₂ emissions and become carbon neutral
  • Conserve resources
  • Provide increased visibility and measurable insights within the facility’s energy management